Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1018 / input capacitance

Guru 11170 points

Other Parts Discussed in Thread: ADS1018

Hi,

How much the input capacitance for ADS1018?

Regards,
Nagai

  • Nagai-san,

    Thank you for your query.

    The ADS1018 uses a switched capacitor input stage as shown in "Figure 9. Simplified Analog Input Circuit"  of the "Analog Inputs" section in the datasheet.

     The input sampling capacitance is a function of the full-scale range (FSR) and the value of the capacitance can be calculated from the Differential Input Impedance provided in the "Electrical Characteristics" table.

    Giving you an example, at FSR =  ±0.256 V, the differential input impedance is 710 kΩ. Since the modulator frequency is 250 kHz, and the differential input impedance is given by 1/(Csampling x modulator frequency), the input sampling capacitor (Csampling) can be calculated to be 5.63 pF. If we add some additional parasitics from bond pad and the input path, 10 pF is a reasonable estimate at FSR =  ±0.256 V. Similarly, we can also calculate the input sampling capacitance for other FSRs.

    Let me know if you have any further questions.

    Thanks,

    Krunal