Other Parts Discussed in Thread: ADC081C027
Hi
My customer is developing their system with ADC081C027. They found a spike voltage at Vin pin.
The spike appears at up-edge of CLK #9 of frame3 in "Figure 30. Typical Pointer Set Followed by Immediate Read of a 2-Byte ADC Register" in the datasheet. The Vin should be about 0.8V constant. The peak voltage of the spike is about 2.2V and the width is about 1us.
The Vin voltage is driven by buffer amp and no spike appears at output of the buffer when the output node is cut. It's means the spike does not come from the buffer.
What is the expected as the cause?
Is ICC of the ADC is increased at the up-edge of CLK#9 of frame3?
Best Regards, Taki