Other Parts Discussed in Thread: DDC114
hi
i could not find detailed information about the complementary inputs of the DDC11* series of ADCs.
the datasheet says "The DDC114 provides optional complementary inputs (DCLK, DIN) to help reduce digital coupling to the analog inputs. If using these inputs, connect a complementary signal to each." which i would read as "DGND level when DCLK/DIN is high and DVDD level when DCLK/DIN is low" i.e. the common ground between the sender and receiver determines the low level.
is this the correct interpretation? if so, how should one generate a complementary clock from a given ttl or cmos clock? something like the obsolete 74265 is needed and all those rs-422/485 drivers would not work(?). a simple inverter would do more harm than good because of the skew between the original true clock and the inverted signal(?)
thanks for any input!