Hi,
We are using same system configuration as described in the conversation from September 9 , 2014 . We are experiencing the same problems. We can add some moe:
We tried to measure a differential analog input +/- 210mVp/1.3 KHz (with DC of 2.5V) with CLK of 25MHz and CLKDIV at High. We got a nice signal at the right frequency but the volatge was 85mVp, we reduce the frequency to 12.5MHz and put CLKDIV al Low, we got a nice signal at the right frequency the voltage was double 170mVp, still not 210mv.
Do you have any idea
Thanks
Amos Oren