Other Parts Discussed in Thread: ADS62P43
We have a ADS62P43 and are attempting to interface it with a Xilinx FPGA development board over a 136-pin Samtec connector. Can we drive the ADC clock (CLKP/CLKM) using a differential clock output from the FPGA over a ribbon cable? What is the appropriate clock input voltage? We have access to 3.3 V and 2.5 V. If these voltages are not appropriate, can an RLC network be added to our PCB to obtain the appropriate voltage?
If the above scenario is not feasible, can we use a CMOS clock source for CLKP/CLKM (as shown on page 47 of the ADS62P43 manual) with LVDS data output?
Thank you for your help