Hi
I'm after some support in designing a filter for the TLC2933A. Its appears to have changed from the TLC2933 and I'm unsure if the calculations still hold true. I need reject jitter as much as possible and any notes etc would be a great help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'm after some support in designing a filter for the TLC2933A. Its appears to have changed from the TLC2933 and I'm unsure if the calculations still hold true. I need reject jitter as much as possible and any notes etc would be a great help.
Yuliya,
Thank you for your interest in the TLC2933A. We will check into the differences between the TLC2933 and TLC2933A and reply to your question as soon as possible.
Yuliya,
Attached is what I have been able to find on the TLC2933A loop filter. It contains a loop filter recommended for the TLC2933A.
Compared to the TLC2933, the TLC2933A has a wider lock range and the VCO gain is different, so the loop filter is not the same.
Other differences:
- The TLC2933A is specified at 3.3V.
- Pin 8 of the TLC2933Amust be connected to GND
Questions about your application:
- Vdd requirements
- Frequency to Fin-A : ? Hz
Hi Larry,
Would seek help in the following:
Customer has an old board designed with TLC2932 , with pin 8 left unconnected.(NC).
TLC2932A , supposed to replace this older chip, and pin 8 need to be connected to GND .
In specific, if using TLC2932A, and pin 8 left NC , what would be the side effects ?
Able to share a rough schematic (internal chipset of TLC2932A), or rough system architecture will do .
This is for customer to gauge effects of any stray voltage /or floating voltage at pin 8 ( if left NC, for TLC2932A)
Thanks.
Hi,
Can anyone here suggest what frequency divider is most suited for TLC2933A??
Warm Regards,
Hadi