Hi,
We have succesfully implemented DAC3484 in an old card, where it was connected to a Xilinx FPGA (Kintex 7). Nowadays, we have decided to use the same device (DAC3484) fed with the same FPGA firmware on a new card where it was still connected to a Xilinx FPGA (however different; Xilinx Ultrscale).
the DAC3484 is configured to drive a real IF carried signal, while driven by a complex baseband signal: functions as an IQ modulator and makes use of the internal PLL as well as of the interpolation chain.
When we observe the analog reconstructed signal (Spectrum analyzer), we notice an impairment symmetric to the "legal" signal with respect to the Fc (center frequency). We suspect that the baseband signal driven by the FPGA is erronousely interpreted, but wonder what it might be due to. Reminder; we use an old debugged firmware.
Might it be due to timing issues of the LVDS data bus? any idea?
Thanks,
Lior