Part Number: TSC2046
Would it be possible to add a minor external load on the internal (buffered) reference?
I would like to add a external 10k or 100k NTC temperature sensor on the aux input via 10k or 100k to Vref.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jose,
Thanks for your reply.
I would like the temperature measurement to be ratiometric. Since the TSC2046 uses single ended conversions on the aux input with Vref as referene to the ADC I thought connecting the NTC as shown below:
I can't find if external loading of Vref is allowed in the datasheet.
Hi Jose,
Happy new year!
I think the auxiliary, internal temperature and battery input channels can only be measured using single ended conversions.
It appears that Vref is always used as the reference for the ADC when singled ended conversions are done. If Vcc could be selected as the reference for single-ended conversion I could simply connect the NTC circuit to Vcc. Since this seems impossible I would like to connect the NTC to Vref so it's ratiometric.
For the "normal" touchscreen channels I use the differential mode with Vcc as reference.
Thanks