Other Parts Discussed in Thread: ADS1298
ADS1298 - I was told via phone that ADS1298 questions should be directed to the Precision Data Converters Forum. But, when I include ADS1298 as the Part Number (above), the Medical Forum is automatically invoked. So, I omitted the Part Number, above.
Hello,
I inherited a design that uses an ADS1298. The device specification indicates the input capacitance is 20 pF (typical), which seems high to me. Also, the spec does not indicate whether that input capacitance represents a common mode or differential value.
Since there is no SPICE model available that I can find for the ADS1298, I downloaded and reviewed the IBIS model. I am not an IBIS model expert, but it appears as though the IBIS model indicates that the analog inputs have a much lower input capacitance than 20pF.
So, I have two questions: (1) Does the specified input capacitance represent the common mode or differential capacitance and (2) Does the specification indicate the incorrect capacitance (or is the IBIS model incorrect or neither of those two things)? Thank you.
Regards,
Don Hall
Medtronic, Inc.