This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5578: Outputcurrent

Part Number: DAC5578

Hi,

I received the following question from my customer.

How much current can the DAC5578 output with all(8ch) channel simultaneously?

Best Regards,

Kuramochi

  • Hi Kuramochi-san,
    Each channel of DAC5578 can source or sink up to 10mA of current.
    Please note that the load regulation spec of the DAC channel is shown in figure 30 - 36 of the DAC5578 datasheet.
    Therefore, the device can consume up to 80mA of current when all eight channels are simultaneously sourcing 10mA of current.

    Best Regards,
    Rahul Prakash