This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Alternate of ADS1298R in a final product

Other Parts Discussed in Thread: ADS1298R

Sir,

I was using ADS1298R Evaluation board for development of an ECG Machine but its user manual states that we can not use it in our end product. Kindly suggest any alternative for that or suggest what can we use for its safety if it is used as it is ?

  • Hello Muhhammad,

    The ADS1298EECGFE-PDK board cannot be used as part of an end-product, but the ADS1298R (the chip, not the board) certainly may be used as part of a product that you design.

    Regards,
    Brian Pisani
  • Thanks sir,

    But I want to know that is there any other board or something else that I may use in addition with this board to confirm safety of the equipment and the patient also without affecting the ECG ? Any isolation board etc ?

    Or even if I use the ADS1298R chip in my design, how can I ensure protection of chip and the patient ?

  • Hello Muhammad,

    I am not aware of any board you can pair with the EVM to ensure that the setup is safe to use with human patients. We did not pass the EVM through regulatory scrutiny for use with real patients so we legally cannot allow people to use it as part of an end equipment - it's only for evaluation of device features an performance.

    The ability of your end-equipment to pass regulatory muster is up to you :-). However, I can tell you that this device was made with medical applications and their various safety and performance standards in mind. We have other customers with products on the market that use the ADS1298R, so it's possible for this chip to be used as an ECG front-end in actual medical equipment that is deemed acceptable by the regulatory agencies in the localities where our customers operate.

    Regards,
    Brian Pisani
  • Thanx Brian,

    It was a great help. Can you please guide that how can we  make the board defibrillator proof ?

  • Hey Muhammad,

    Protecting the circuit from defibrillator shock can be done using diode circuits - similar to other types of overvoltage protection. Typically this can be done with a bidirectional diode, with one shunting the input to AVSS and the other one shunting the input to AVDD. This way if the input voltage goes a little above either rail, it will get clamped before exceeding the maximum voltage for the chip.

    Regards,
    Brian Pisani
  • Thanks Brian for your help and suggestions.