Part Number: ADS1263
Other Parts Discussed in Thread: THS4131
Hi,
if I use +5V external reference, to measure +-5V pesudo difference singnal,how to design the circuit?
Thanks,
Junhua
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Junhua,
In order to measure a +/- 5V differential signal with the ADS1263, the signal will need to be fully-differential. In other words, the input signals must mirror each other around a mid-supply common-mode voltage. For example, if the ADS1263 is operated off of a unipolar 5V supply then:
+5V differential input requires: AINP = 5V, AINN = 0V
-5V differential input requires: AINP = 0V, AINN = 5V
You might consider using a fully-differential amplifier to convert the pseudo-differential signal to a fully-differential signal, as shown below:
The main problem with the above circuit, is that the output becomes nonlinear near the supply rails. Therefore, you may need to support a wider supply range and use a similar circuit with a higher voltage amplifier, such as the THS4131.
Best Regards,
Chris