Part Number: DDC1128EVM
Dear Sir/Madam,
Currently we are evaluating a DDC1128 Current-Input Analog-to-Digital Converter using the DDC1128EVM evaluation board. I would like to convert the raw output codes to a current in A (nA, uA, etc.). I can’t figure out how to calculate this.
This is how I tried to calculate it:
- Full-scale 100% is equal to 150pC according table 7 in the datasheet.
- 100% is equal to 0xFFFFF (decimal 1048575)
- 150pC / 1048575 = 0,000143051284 pC/step
- Capture data using the PC software, this gives me a raw value of e.g. decimal 4011
- 011 x 0,000143051284 = 0,57 pC while the PC software says -0,01220 pC. What am I doing wrong?
Does the Vref influence the value in Coulombs? I am using the onboard reference (REF3040, 4.096V).
Using the value in Coulombs and Tint (integration time), the current in Amps can be calculated.
So in short: What’s the equation for converting the raw values to amps?
Thank you very much in advance!