Part Number: ADS1259-Q1
Other Parts Discussed in Thread: INA240, ADS1259, OPA376-Q1, ADS1120-Q1
Hi teams,
I have a customer who is thinking about designing a system using the ADS1259-Q1 to sense current. The current shunt amplifier will be the INA240. You guys don't see any issues with that part driving the ADC directly, do you? Likely they will be sampling at about 1ksps. They are doing high side sensing, and the output of the amp could be 0V-1.5V across their current sensing range.
Also, it looks like the ADS1259-Q1 is dual supplied for both the analog and digital. Since the processor will be on 3v3, but the part's analog supply really needs to be at 5V, can the part handle both 3v3 on the digital and 5v on the analog? I just want to make sure that there's nothing funny with latchup/level shifting that may impact the operation of the part.
Thanks,
Brian