Hi ,i am using AFE4300 EVM PDK kit for body composition measurements like to measure FFM TBW FM ECW and ECE. I have few question regarding AFE4300 EVM PDK kit.
1.In AFE4300 why we connect 1kohm impedance resistor between IOUT0 and IOUT1?
2. In AFE4300 GUI calib const.ini setting there is 32 frequency for FWR and 8 16 32 and 64 frequency is for IQ ,whether this frequency is in hz or kHz?also i need to change these frequency between range 5to 500kHz then what will be the clock devider?for 8 frequency there is 10240 is clock devider then for 50hz frequency what will be the clock devider please give me detail calculation about this.
3.if we connect wire between j40 and j30 and place shunt across j10.then remaining four terminal of j38 where to connect on human body to inject current .please provide me the position of these four terminals.