Hello,
I just got the AFE4300 sesnor up and running with an Arduino DUE. It all works fine from a flow perspective but I see some inconsistent behavior on weigh scale front.
1) The adc values read for same voltage (12mv) ranges from 330 - 550 am not sure why this is happening
2) When I try to measure the voltage using a multimeter, the VLDO goes off!!! if I hold the multimeter before I turn on weight scale front end, then no issues I read 1.7V always but if I try to put the multimeter after the front end is on and try to measure, it goes off!!! and I read 0.0 on ADC (Really strange)
Can you please help me in this regard?
regards,
Shankar