This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7822: Thermal Pad Connection

Part Number: DAC7822

Hi,

The datasheet does not specify the connection of the exposed thermal pad. Is it N/C or ground, maybe neither? My gut tells me to connect it to the ground plane for thermal dissipation but I wanted confirmation.

Thank you,

Ryan

  • Ryan,

    In general thermal pads should always be connected to the lowest / negative most potential used by the device, which in the case of a single-supply product that would be ground. Being that this is an MDAC and therefore basically just an R-2R ladder internally without any internal reference or output amplifiers the overall heat dissipation of the device is quite low so I wouldn't say that utilization of the thermal pad is required. From a mechanical stability perspective, however, I think it is always advisable to use the thermal pad, especially on modern thin QFN packages.

  • Hi Kevin,

    Thanks for the quick reply! Since you recommended connecting this pad to the lowest potential (which might not be ground in a split supply application), would I be right to assume this pad is not internally connected to the device ground and is just a N/C?

    Thanks,
    Ryan