Part Number: ADC12D1800RF
Other Parts Discussed in Thread: ADS4149EVM, ADC12D500RF
HI, this is Jun Hee Cho.
I have some questions.
Before I ask a question
First, I will briefly explain the application we are going to develop.
We want to find bio-signals wirelessly through RF signals through antenna and convert the datas using ADCs.
The center frequency of the signal I use is 3 ~ 5GHz and I am looking for an ADC with a bandwidth of 3GHz or more.
The input signal has a pulse repeating frequency (PRF) of 1 M to 10 MHz.
I was looking for a product called ADC12D1800RF.
It has a maximum bandwidth of 4 GHz and a minimum sampling frequency of 500 MHz.
We use a PRF of 1M to 10MHz, and wonder if the ADC's input does not operate at all if the input is less than 500MHz.
If so, I know that the ADC has a driver circuit that receives the CLOCK signal. I wonder if this driver circuit does not work if a CLOCK signal of 500MHz or less is input.
In addition, if there is an ADC that meets these specifications, I want to know what it is. I would like to know if there is an FPGA that can transfer the ADC's output data to a PC.
PS. I am already using the ADS4149EVM and the minimum sampling clock signal on this board is 20MHz. But I use it at 1MHz ~ 20MHz. Because of this fact, I asked the above question.
thanks.