Part Number: DAC5672
Dears.
We are considering DAC5672.
What is the function of the DE-MUX?
A detailed explanation is necessary for Block Diagram.
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC5672
Dears.
We are considering DAC5672.
What is the function of the DE-MUX?
A detailed explanation is necessary for Block Diagram.
Thank you.
Henry,
The De-Mux allows the device to operate in a single-bus interleave mode. Both CHA and CHB DAC's input data will be interleaved on bus DA[13:0] in this mode. DB[13:0] is not used. To activate this mode, set the MODE pin to GND. See the section called "Single Bus Interleave Data Interface and Timing" on page 14 of the data sheet for more information.
Regards,
Jim