1: I have a project where I need to convert legacy video signals such as CVBS NTSC and PAL, Analog and Digital RGB, and VGA to HDMI. I believe the TVP5146M2 is the current part that would best fit my needs of getting the signals to digital. Can someone please confirm this? I do know the TVP5146M2 does not output to HDMI and I need another IC for that.
2: I then would like to ask about CVBS NTSC input, and Analog RGB input with a Horizontal Scan Frequency of 15.700 kHz, and VGA at 15 kHz. These are slightly lower than what is usually standard. Will there be any issues when using the TVP5146M2? Can I set the registers to sync and lock correctly to the non-standard frequency? Or does the IC lock automatically after some time? Or will there be need for some extra configuration or parts involved?
3: Lastly, I noticed the TVP5146EVM-TVP5146 Evaluation Module is out of stock. Is this the board I should use for testing or is there something that supersedes it? If I place an order then how long typically is delivery on out of stock items?
Thanks in advance for your assistance,. and I look forward to a response.
Henry