This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8562: How To Connect CLR if Not Used

Part Number: DAC8562


Can the CLR_B pin be connected to ground if the CLR functionality is not used? I assume I can, but it is not 100 % clear from the data sheet, since there it is only mentioned that the CLR_B input is 'falling-edge sensitive'.

Thanks for a short reply.

Patrick