Part Number: ADC12D800RFRB
Hello,
I have a ADC12D800RFRB and want to do some development using it. But I notice that the documents provided on the website (www.ti.com/.../adc12d800rfrb Documents) are inconsistent with the board I have.
The reference board has a FMC connector on it, which is the same as the one in snau146. However, the schematics in the design package does not have it. Instead in the schematics there is a 38 pin MICTOR connector. So it seems the documents in the reference board design package are outdated.
Where can I find the latest design package for ADC12800RFRB? Thanks a lot.
Edit: I just found that the design package for ADC12D1800RFRB has a text file in it saying the schematics in it is also for ADC12D800RFRB, so the schematics is found. However the there is no FPGA code for ADC12D800RFRB, so where can I find the FPGA code for ADC12D800RFRB? Thanks!
Lingmei