Part Number: ADC1175
Support Path: /Product/Device selection assistance/
Hello,
I have an application for an 8-bit ADC, but it is low-speed. I like the specifications of the ADC1175 because of it's parallel output and two reference voltage inputs. However, I can only provide a clock signal up to 100KHz. Will this work as a clock speed even though it is outside the recommended range?
thanks,
Greg