Part Number: ADS7223
Other Parts Discussed in Thread: ADS8586S, ADS8588S, AMC1100, ADS7253
I need to monitor voltage and current on high voltage 3-phase ac line circuits. Therefore, I would like to use three separate ADS7223 to make three dual simultaneous reading (2x3=6). I only have one 4-wire SPI buss available (BeagleBone Black) but I do have individual GPIO that can be used for device selection. My sample (conversion) rate is 500us (0.5ms).
1. Is this possible?
2. What connections to SPI bus need to be made?
3. What mode is best for this operation?
4. Is the ADS7223 the best choice for this application?