Other Parts Discussed in Thread: ADS5560
I am using the TMS320F28377S for test but its ADCs on chip are not satisfied, for example SNR at higher frequency.
The input signal:
Sine wave
Frequency 10 MHz
Amplitude 1 V
Resolution requirement 16 bit
Single end input
In TI's high speed ADCs there are no single end input ADCs. The speed of ADS7042 is lower. Are there any suitable products in precision ADCs.