Part Number: DAC8750
Hello,
I need your help to calculate the total unadjusted error(TUE) for Iout over temperature. The TUE mentioned in the Electrical Characteristics table is +/-0.16FSR, but based on the datasheet graphs I believe the device can perform better in my application. I'm not 100% sure which graphs I need to calculate together.
In my application the output range is 4-20mA, internal reference and internal Rset are used and analog Vdd is 24V. I'm looking for a maximum error over the temperature range of -20C to +65C? For example, what kind of error I can expect to see when I program the output for 20mA?
I may need to implement calibration depending on the result.
Thanks in advance!