Other Parts Discussed in Thread: ADS5463, ADS4149EVM, ADS4149, ADC12D500RF, ADC12D800RF, ADC12J4000EVM, ADC12J4000
Thanks for the answer.
I just want to ask you one more question.
The ADC of the ADS5463 has a bandwidth of up to 2.3 GHz,
It has a clock input range of 20 ~ 500MSPS.
I would like to use 1M ~ 5Msps sampling clock, but I wonder if adc will work in this environment. You do not need to have high performance.
Previously, the ads4149evm I was using had a clock input range of 20 ~ 80Msps, but it worked well at 1Msps.
So I think it is also possible with ADS5463.
I wonder if it is an ADC that can not accept clocks below 20Msps.