Part Number: ADS7044EVM-PDK
Hi all,
I currently working with the ADS7044EVM-PDK and ADS7042EVM-PDK. As I update the firmware in EVM SD card, the EVM-PDK can only be recognized as BULK DATA interface which is Mass Storage device.
This cause the ADS704X EVM GUI can actually tell the EVM is 7044 or 7042, but it just frozen afterwords. I guess it's just waiting for the response.
Did any of you meet the same problem before and get the solution. Or if we can be provided the necessary firmware for the SD card file. Right now I'm using the SD card File provided by GUI.
Wenbing