Part Number: ADS42JB69EVM
Other Parts Discussed in Thread: LMK04828, ADS42JB69
I have a question with using the ADS42JB69EVM with the TSW14J56. I have High Speed Data Converter Pro v4.50, ADS42JBx9 GUI (8/15/13) and the Clock Design Tool software installed.
My question is how to change the sample clock frequency. In the HSDC Pro program, I can set the ADC Output Data Rate, and it displays a message to set the ADC clock to match. I know setting the ADC clock is done via the ADC GUI tool, but how to determine the new values? It appears the recommended method is to use the Clock Design Tool. To get a baseline, I tried setting output frequency in the design tool to match the default value set by the ADC GUI (250 MHz), which results in VCO settings that don't match what the GUI is using. If I manually enter the PLL dividers used by the GUI, the output frequency does not match and some of the boxes turn red (out of range). I would appreciate any guidance from someone who has been through this process before.
-Bill