Part Number: ADS1293
Having killed a couple of ADS1293 chips during development, I'm concerned about possible latch-up and/or power feed-through via the electrode input ESD protection diodes. The failed devices exhibit a very low resistance between the analog Vdd and Vss pins.
I suspect voltages in the +/- 20 Volt range may have been present on INx input pins both before and during power-up.
The datasheet lists absolute maximum ratings for the input pins, but no explanation of behaviour outside this voltage range, other than the ESD ratings for much higher transient voltages
Is there a Spice model of the input protection structures?
Alternatively, are there any specifications for maximum tolerable input pin current under such fault conditions, or recommendations on preventing damage (I already have 10k in series with each input to limit current, but no other external protection circuitry) ?