why are there two TVS diodes in typical application circuit of page 36? The right TVS is turned on, and the IOUT is shorted to the ground. The IOUT cann't ouput 4-20mA, can it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
why are there two TVS diodes in typical application circuit of page 36? The right TVS is turned on, and the IOUT is shorted to the ground. The IOUT cann't ouput 4-20mA, can it?
Hello,
I suppose the answer is that it depends on the diode.
Some TVS diodes are constructed as, basically, a zener diode with a series standard diode facing opposite directions. In such a structure the zener does not break down until the required reverse breakdown voltage is applied along with the forward voltage associated with the series standard diode. In the other direction the standard diode must achieve reverse breakdown for conduction to occur, which is generally a fairly high voltage.
It comes down to what is in the particular diode datasheet. If the TVS diode is not constructed as described above and had low forward voltage then your statements are true and the diode would conduct once the voltage at IOUT were sufficiently high to forward bias the diode on the right.