This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8814EVM: DAC 8814 EVM not working

Part Number: DAC8814EVM

Hello,

                   We have brought a DAC 8814 EVM. I have been trying to drive it , but it was not working. I have tied MSB pin (J1.1) to GND and have given all power supplies as follows. I checked the voltages using the multimeter also.

J3.1                      +15V

J3.2                       -15V

J3.3                        +5V

J3.4                         -5V

J3.5                         GND

J3.6                         GND    

J3.10                       5V

When I switch ON power supply, board is ON and  all channels show 5V output voltage. When I connect   reset pin (J2.T 19) to ground also I get 5V only in all channels. Board dont reset.

Jumper settings are :

SW1-SW4  : LEFT

W1-W4       : 1 AND 2 SHORT

W5-W8       : 1 AND 2 SHORT

W9 ,W10    : 1 AND 2 SHORT

Please help me in finding why this happens so and help me solve problem.

With Regards

Shalini