Hi All,
While my boards are out for fab, I'm working on the library to access this ADC. Unfortunately I cannot get it to respond to any i2c queries (either directly to address 0x54 or by scanning all addreses looking for ACK). I have the chip on an adapter board in my breadboard at the moment.
I have the SDA, SCL pulled up to 3v with 10k pullups and have the recommended "typical" application circuit breadboarded (except for a 4.7uF ceramic cap instead of tantalum).
I'm trying to rule out a DOA, static damage, or infant mortality. I'm working with the 6 pin sot23-6 package and there is no pin 1 marker on the chip. I set the orientation so that the pin below and left of the start of the marking was pin 1. Getting no response, I rotated the chip, but I don't know if the SDA and SCL pins can handle the 3v and ground applied to them.
Am I missing something obvious here or did I fry the chip? (I got the chip directly from TI as a sample so I'm sure it is genuine.
Thanks