Part Number: ADS4229EVM
Other Parts Discussed in Thread: ADS4229
I am using ADS4229 EVM. This is my test specifications:
Signal generator CH1: 800mV, 4MHz,Sine wave, 50 Ohms connect to ChA on ADS board (J6)
Signal generator CH2-Sync: 800mV, 8MHz, 50 Ohms connect to CLK on ADS board (J19)
Power supply 5V to ADS board
At J1 (Data out), I did not detect any signal. Please help me debugging this problem. I was able to see input signal and clock coming into the board btw. Thank you.
Lac