Part Number: ADS131A04EVM
Other Parts Discussed in Thread: ADS131A04,
Hi,
I have a problem with setting up the ADS131A04. I use the ADS131A04EVM, but connected the SPI lines to a Raspberry Pi. Reading and Writing the registers works fine. I'll use the asynchron slave mode, and also the interrupts are generated (by the ADS131) and received (by the Pi) without problems. Following data sheet figure 109, I set some registers I need, enable ADCs, send wakeup and lock the registers. Every command is acknowledged as expected. But - there is no conversion value in the frames I read. I connected only J7 of the EVM (n-input about 1.3 V, p-input about 2.0 V), the remaining inputs of the EVM are open. I would expect quite accurate values for the used input and some small noisy values on the others, but I read simply "0" for all bytes. The registers 02h..05h don't report any error. What happens here, what do I miss? Is it possible to destroy the analog inputs in a way the digital output is constant "0".