Part Number: SM73201-ARC-EV
Hello,
I am trying to acquire data using the provided Arc Detection Interface v1.14 application. I am able to connect to the GUI through the RS232 interface, and have verified the connection works via terminal. When I try to capture data, I am immediately presented with a blank graph, or occasionally a graph with very little data. I also sometimes get various error messages. I have only once been able to acquire expected waveforms (did not screenshot). I have attached screenshots below.
I am also wondering about the "RD195 acquire mode" checkbox which is not mentioned anywhere in the manual, nor is it in the manuals screenshots. Should this be checked or unchecked?
Any help in solving these issues would be appreciated.
Thanks,
Matt