Other Parts Discussed in Thread: XTR115, DAC7750, DAC8750, DAC7760, DAC8760, DAC8775, TIPD101, TIPD102, XTR117, TIPD158, XTR116, DAC161S997
I want ro produce a double/dual current output (4-20 mA) with a common Mikrocontroller (e.g. Atmega) from a sensor signal.
One Output can be source type and one sink or both should be sink type. The value of both outputs should be the same.
I have some ideas how this issue could be solved:
- current loop transmitter (sink type) via PWM control [like XTR115 but as a sink; I/I amplifier?]
- voltage controlled current source/sink via PWM control [U/I converter?]
- DAC with double current sink output via SPI [DAC]?
Power supply: 24 VDC
What is the best/ cheapest way? What are appropriate TI products?
best regards,
Erik