Other Parts Discussed in Thread: ADS124S08, ADS1274, ADS1220
Hello, I am a university student working on a Capstone project involving the use of 4 load cells in a full wheatstone bridge configuration. I do not have much experience with analog design so please forgive me if my question is very simple or misguided. I plan on using the the 4 differential inputs of the ADC to simultaneously sample the 4 load cells. Without any prior signal conditioning or amplification, should this be signfigant enough to measure signals in the 10 mV range? Another question I have is about the 60-Hz attenuation, is the 20 SPS stated in the datasheet for the multiplexed signal? i.e., to get good 60-Hz rejection can each channel only be sampled at a maximum of 5 SPS? (20 / 4 channels)
Again I apologize if this question is very simple, or is misguided, this is my first real experience with any sort of analog design. Any help would be greatly appreciated!