Hello,
I'm currently working in a design that uses two ADS8558 connected in Daisy Chain and configured to be in Software Mode. According to Figure 42 in ADS8558 datasheet, a Busy signal pulse should be seen after a reset signal while nFS is high. Currently I can't see that initial pulse to start the configuration through SDI, am I misinterpreting the Datasheet? I don't see any Busy signal when a Convst_A is generated either. Please, could you review my Schematic and tell me if I did something wrong with the connections? Signals 3COM and ACOM are return signals and are connected together, they have different names only for reference.
Thank you.
Jorge Corro