This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM: High Speed Data Converter Pro "no firmware please select a device to load firmware into the board" error

Part Number: TSW1400EVM
Other Parts Discussed in Thread: AFE5809EVM, AFE5809

Dear All,

I'm using TSW1400evm Rev D and AFE5809EVM Rev. A. Following the User guide instructions, I setup AFE5809EVM GUI properly. Then, I open High Speed Data Converter Pro (V 4.5) and connect to the board. After that, I select my AFE5809_14x from the top left menu. Then for a few seconds, it shows the message that the firmware is downloading. However, the process is interrupted with the following error:

"no firmware please select a device to load firmware into the board".

After trying the same process on another PC, I noticed that I could successfully load the firmware into the board. However, on the new pc, the same error occurred a few days later. 

My issue is exactly same with the issue on the following thread. Do you have any suggestions on how to fix this issue?

e2e.ti.com/.../1136170

Thank you.