I have a customer who has some questions about the CLK input. The data sheet states that you should use a high-quality low-jitter clock source as this clock controls the operation of the entire chip. But it does not give any details. Please look at the customer’s issue below:
I would like more detail about the requirements for the main clock that has to be supplied to the ADS1271. Specifically, does the duty cycle of the clock matter (does it need to be 50%)? Does it only require evenly space rising edges, or do the falling edges need to be precise and consistent as well? Due to a design mistake, I find myself unable to synthesize the exact main clock frequency required for my chosen SPS. I may be able to make one with a different duty cycle, though.
I did not know how to answer this as there are no duty-cycle limits listed in the data sheet and there is not an explanation of how the ADS1271 uses the rising or falling edge internally. Can you comment on these questions.
Thanks for your help with this!
Richard Elmquist