Hello,
I am trying to use the ADS42LB69 in DDR mode, but with only a single channel. THe datasheet seems unclear to me as to how to do this; I thought I could just use the CTRL pins to disable the unused channel; but this table has be confused. From the device datasheet, page 43, it shows:
which seems to state that I CANNOT power down channel B in DDR mode?!?!? So, if i want to use a single channel in DDR mode, am I forced to use channel B; because A is the only one you can power down? That's not intuitive; and doesn't seem to jive with the rest of the datasheet that shows the two channels as basic mirrors of one another- is this table just hosed up?