Part Number: TSW1405EVM
Other Parts Discussed in Thread: AFE5808AEVM, AFE5808A, AFE5808
We are trying to interface AFE5808AEVM with TSW1405EVM.
Older thread: https://e2e.ti.com/support/other_analog/imaging_afes/f/239/t/407866
- As per both related devices section of TSW1405EVM, only ADS12* series products are mentioned as compatible. Are these two compatible?
- We followed the user guide of AFE5808AEVM on interfacing with TSW1400EVM
- We connected +-5V (current limited at 1A) to AFE5808AEVM connected with TSW1405EVM, both connected to a Windows 7 PC via USB cable.
- Both boards are getting recognised in corresponding GUIs.
- We choose onboard 40MHz clock and gave 2MHz 600mV pk-pk sine wave as input to channel 2 on AFE
- On the AFE GUI, we set Single to take on board CLK and then choose test pattern as ramp
- As mentioned in Section 7 (page 8), High Speed Data Converter Pro GUI version is v2.7, from which they could select AFE5808A board. But the current available version of HSDC Pro is v4.5 which does not have option to select AFE5808A.
- As per the older thread mentioned above, there was a suggestion to use ADS528x and set LSB first in ADC settings and also reversing the order of the channels (1-->8 , 2-->7 etc) by a user.
- We didn't quite understand the reversing channel part. Is this a verified workaround?
- Is it possible for TI to provide an updated user guide or ini file for AFE5808A to be used with HSDC Pro v4.5 and TSW1405EVM?
- In the screenshot of HSDC Pro GUI (page 11) provided with AFE5808AEVM user guide, on the bottom status bar, Interface Type = ADC_FIRMWARE is given. It is not shown in our installation.
Please let me know if any further details are required.