Part Number: ADS1298
I have a very specific question on the ADS1298 that doesn’t appear to be answered by the data sheet. On page 42 of the spec (http://www.ti.com/lit/ds/symlink/ads1298.pdf ), there is a drawing of the Right Leg Drive provisions of the ADS1298. In short, 220Kohm resistors from each of the 8 channels are mixed and inverted by the RLD amplifier. The gain of that amplifier is set externally by the ratio of an external resistor (likely metal film) chosen by the designer and the 220K internal resistor (or 220K/channels mixed). My question; Are those resistors ordinary silicon resistors (+/- 30% tolerance) or are they an improved configuration with less drift that the simplified drawing can’t show. If the former case is true, the RLD amplifier will experience a significant amount of CMRR drift. Would appreciate an answer. Thanks.
Pete Vander Jagt
DornerWorks Ltd.