Part Number: ADS8318
Greetings,
We have Technical Query on ADS8318IBDGS. which is considered in one of our design and we need the data urgently to support the design requirement.
Query:
a. As per datasheet: Max Tj = 150°C & operating temp range (-40 to 85°C), Could you please confirm is it air temp, case temp or junction temp.?
b. Please do provide the reliability /qualification reports available for this part?
c. Power dissipation expected during the specification sheet test?
d. As per datasheet RθJA = 180°C/W, we would like to know the RθJC ?
e. If there are different temperature rating, are they all the same die design?
f. Any parameter information with greater 85°C?
Your quick reply in this regard will be highly appreciated.
Thanks
Siby