This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5809EVM: Saving converted data into file from High Speed Data Converter Pro software

Part Number: AFE5809EVM

Dear All,

We are using AFE5809EVM + TSW1400EVM to convert input analog signal into output digital signal. I can successfully capture the digital signal output and display it inside High Speed Data Converter Pro software. I can even export the data by right clicking on the data and then exporting it for excel. I would like to know if it's possible to automatically export the data to a file. If this is possible, then I can ask my code from another software (such as matlab or labview) to access that file and use the data for signal processing.

Any advice is highly appreciated.

Thank you

  • Hi Sajad,

    You can use the ADC Temp.bin file for accessing the data in HSDC Pro from another software. The byte order of the data in the file is little-endian.
    The ADC Temp.bin will be located under C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro