I measured the ads1292 voltage value
VDD 3.3V
VREFP 1.5V
VREFN -1.5V
VCAP1 -0.6V
VCAP2 3.4V
Register configuration :
config1 0x02
config2 0x80
Channel1 0x01
Channel2 0x01
I got the ads1292 datas and annalyzed it, but the offset measurement result I can not accept. I attached the test result pictures for channel A and Channel B. what's the problem?
Schematic