Part Number: ADS1120
Hi everyone!
Is there a limitation of capacitance that the included current sources can handle? I do not find anything in the datasheet about this (or I'm just blind). Bob, if you read this - we once talked about this application as shown here:
This is indeed not a common application, but I needed it for rough temperature measurements and it works very well. I also added the two red capacitors and did a lot of tests and measurements and everything worked really good without any oscillations. I'm sourcing a current of 100µA out of AIN0 and also using this pin as REF+. Then I use AIN3 as REF- and I also sample AIN3 against AVSS. From the performance point of view this is surely not the best thing, but I do not need very precise results at all. The other channel is important for me (not shown here). Temperature is just a side info and can be wrong for a few degrees. But now I was wondering if there is a limitation of capacitance the current sources can drive since there is no information about the working principle of the current sources. Is there any known limitation? Honestly this is just for my personal information because there is not actual problem, but I would be interested to know.
Dennis