Part Number: DAC3162
Other Parts Discussed in Thread: DAC3174
Dears.
What is the role of the Transformer in connection with DAC3162's IOUTP?
Should I use a Transformer?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The transformer is doing a differential to single ended conversion into a 50 ohm load so that you can take the EVM output to standard bench test equipment such as a spectrum analyzer. There is also the option on the EVM to remove the transformer and install the second SMA output for a differential output if you wished. And on some other DAC EVMs that you may look at you may see that the differential outputs may go to a modulator device, and in those EVMs you would see a typical example of a differential DAC output to some other device input without the transformer. (But even then on those EVMs the modulator output may be transformer coupled to provide a single ended output from the EVM again. The DAC3174 is one of those other EVMs with the modulator output for example.)
Regards,
Richard P.