I am looking for a graph of TLV2556 input impedance over temperature. Also what is the recommended drive circuit for this device? Does TI have a recommended R & C flywheel filter?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am looking for a graph of TLV2556 input impedance over temperature. Also what is the recommended drive circuit for this device? Does TI have a recommended R & C flywheel filter?
Hi Tim,
We do not have a graph relating the input impedance of the TLV2556 over temperature. The switch resistance (worst case) is 600 ohms with a 55pF sample/hold capacitor and the acquisition time is based on how the device is configured (8, 12 or 16 SCLKs). Going with 15MHz clock and 8 cycle sampling, you have ~533nS acquisition time. You'll be looking at an amplifier with ~11MHz GBW. As a starting point for R and C, you might consider ~56ohms and 1.1nF. The following documents should help you out in trying to find the optimal solution: